USB Battery Charging
The more I read about USB battery charging, the more questions I have :.) First question, does T.I. have a self enumerating USB battery charger chip? So far, I have only found one company that makes a self enumerating USB battery charging chip and unless I’m missing something, it isn’t as “smart” as I would expect. First it uses resistor and current sink techniques to determine if the host is a dedicated USB charger, a charging downstream port or a standard downstream port. If it determines it is a standard downstream port, it will communicate with the host and enumerate. It will request 500 mA, if request is denied, it will default to 100 mA and set the charger chip input current limit accordingly. For the “smarts” to be able to enumerate, this seems not so smart to me. Let’s say the host couldn’t provide 500 mA but it could provide 400 mA. I would think it would make a lot more sense to then “agree” with the host on 400 mA and set the input current limit to 400 mA.
The device that I am developing does not have a microprocessor but it does have a 1 Amp Hour Li-ion battery. For simplicity, I will use the term “full charge” as the time from fully discharged until the 4.2 Volt switch over to constant Voltage mode. In other words, a 1 hour “fast charge” at a 1C charge rate. So at 100 mA, it would take 10 hours but at 400 mA, it would only take 2.5 hours (assuming the device is off during charging and 100% of the current is used for battery charging). That is a fairly big difference.
To further complicate matters, a USB 3.0 standard downstream port can supply 150 mA minimum and 900 mA maximum. So a “smart” self enumerating Li-ion (or LiPo) charger I would think should be able to set the input current limit at 100 mA, 150 mA, 200 mA, 300 mA, 400 mA, 450 mA, 500 mA, 600 mA, 750 mA and 900 mA to be able to fully optimize charging from USB 2.0 or USB 3.0 standard downstream ports as well as set higher currents for charger downstream ports and dedicated charger ports.
Am I missing something here in my thinking? Does T.I. make a stand alone charger chip that can do this?
Martin Risso