Hi,
Do we have an estimated value of efficiency for the TPS92691-Q1 in a Sepic topology for the two below scenarios:
- Scenario 1:
Input voltage 9 V to 16 V from -40°C to 60°C
Output max 60 V 60 W - Scenario 2:
- Input voltage 9 V to 16 V from -40°C to 60°C
Output max 30 V 15W 500mA
Do you have another reference for lighting row LEDs ?
Thanks and regards,
Mohamed