Part Number: LM5007
Hello,
since some weeks we are faced with the problem that the flyback diode of our LM5007 dc/dc converter circuit gets broken at our customers system.
But we weren't able to reproduce it at our lab so far.
Our electronics (~100 pcs) works for months 24/7 without any failures.
This is what our 5V voltage regulator looks like:
The only difference is, that the flyback diode D4 is a 60V/1A type (10MQ060NPbF).
The input voltage (HV-IN) is 48V, maybe 52V, and the 5V load appr. 400mA.
We have an almost exact circuit at the same board with 12V output voltage, but until now we received only five defect 5V flyback diodes.
We already noticed that the maximum voltage rating of the diode (60V) could be a problem. But we analyzed the real breakdown voltage and it amounts very reliable 78V.
And since weeks we run the electronic in a climate chamber with 60°C at 58V without any failure.
Does anyone have an idea what might be the reason for the defect diode?
We noticed a negative spike for maybe 2ns of about -5V (load dependent) at the flyback diode (SW node) after control-FET turn-off. Maybe this is a hint.
We are thankful for every idea! Tomorrow we analyze the broken diode in a xray lab. Maybe this shows us the failure cause.
Best regards,
Sven Langhoff.