Hello team,
I am looking for a solution recommendation for the following specs:
Input Voltage: 85 - 305 VAC
Output Voltage: 56 VDC / 120W
Careabouts: low cost, space (size similar to or smaller than PMP4334), EMI Performance
It seems like the PMP4334 Reference Design is a close fit, but I was wondering if there is any recommended solutions that would be an integrated PFC + DC/DC Combo (because of of space and cost restrictions).