This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61070: quiescent current?

Part Number: TPS61070


There is no load at the output. Thinking this must setup the chip to its quiescent state. I'm getting a measurement of ~350uA when putting a DMM in series with the positive side of the battery connection. I should be reading something lower, like less than 50uA.How do you recommend measuring quiescent current? Running 2-AA, using Wurth 744031004 inductor, 1 mega ohm, 180k, 10uF 0603 ceramic caps for both input and output. Getting 3.3Vdc at the output, so that looks good. Just concerned that I might have something wrong if I'm getting the higher than documented quiescent current.

Thanks for you help,

Alex