This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62569: TLV62569 input short & damage

Part Number: TLV62569

Hi All,

My condition : Vin = 5V , Vout = 1.2V, Iout = 300mA

I have test, It will short input, When load = 300mA

This is my circuit.

When input short, It have reverse current 8A. IC will damage. Do you have any solution could reduce or prevent this problem???

What is high side MOSFET max current??