Hi.
I am testing the LMR16030. But there is a problem.
WEBENCH® Designer designed and implemented the circuit.
However, resonance noise is occurring. What is the cause?
Please check whether there is a countermeasure.
--> Design Spec
Input: DC 12V
Output: DC5.4V
Load: 1A under
SW Pin ( Before Inductor ) Waveform
After Inductor ( Load ) Waveform
Thanks.
Regards,
Tyler