This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: bq34z100-G1 TrueFCC & TrueRC jump,then SOC drop quickly

Part Number: BQ34Z100-G1
Other Parts Discussed in Thread: BQ34Z100EVM

Hi

I have complete learning cycle and update-status became 06 automatically. Then I use current@1C to discharge. TrueRC and TrueFCC jump abnormally.

When SOC=83%, TrueRC and True FCC suddenly jump from 4864mah to. Then, TrueRC and TrueFCC go back to normal slowly until SOC=54%. But, SOC drops smoothly so quickly from 83% to54%.

I have test many times , SOC/TrueFCC  always jump at around 70% ~80%. Why?  What reason can cause?

Thanks!   log-data.zip

  • Hi,
    Could you upload your log data when you test the chem id of the battery?
    Also the log data when you doing the learning cycle?
    I have a battery on my hand and a bq34z100evm, could you kindly share your srec file and I will program your srec file into my EVM and see what is going wrong.