Hello,
I have a couple of questions about BQ24297:
1) Table 2 on the data sheet states that OTG is used for selecting between 100 mA and 500 mA when a USB host is connected, but is the OTG pin only used for USB on-the-go mode? As I don't need this mode, can I ignore that pin and tie it to VDD or GND?
2) I find shipping mode to be a very interesting feature, but it is not clear to me whether it can be used when battery is the only power source in the system. I would like to use the available ON/OFF button to go into and exit shipping mode, but the data sheet in section 9.3.1.2.2 states that "system voltage is zero". Does this mean there would be no way to "awake" the system without an external power source?
Thanks in advance.
Regards,
Stefano