Other Parts Discussed in Thread: TPS61196, TPS61199
Hi.
Configure the circuit using TPS61196-Q1 and inquire for problems during TEST.
Design
1. We connected the TPS61196 in series with 23 LEDs per Ch.
2. The Ilim setting is set to 50mA and the PWM duty is set to 20mA output.
3. Vh is 90V.
Issue
1. I made 20 sets and I lost 3 ICs of TEST.
2. Even when the PWM is in the 0 state, the LED light is intermittent.
Question
1. I wonder if the above symptoms are caused by high voltage of VFB.
2. Can you check if there is a solution that can drive 23pcs RGB LEDs per Ch with 20mA using the TPS61196?
I will wait for your reply.
Thanks,
Regards,
Tyler