This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2576: LM2576-ADJ feedback and output pins at almost same potential

Part Number: LM2576


Refer the schematic below, supposed to generate 15V DC output @1Amp for 28V DC input from external SMPS source. But multi-meter observes constant output of 1.3VDC while feedback pin voltage is observed as 1.2VDC. Verified with two different LM2576-ADJ  parts, behavior remains same. Any advice !