Part Number: LMG3410
After reading advance info/datasheet and some details, I was wandering if this device can be used in full bridge mode to generate +400V /-70V drive --- Yes I am interested in in positive 400V and negative 70V .
I am thinking about driving capacitive load of about 450nF up to 400hz in sinusoidal drive...
Are there any limitations ?
Can we use the same device to generate 400V /-70V as well ?
is there a way to configure it to make it work in like class D amplifier to save power ?
K B Shah