I am considering using your TPS2H000-Q1 as a current-limiting device for a power supply that could range from 5V to 16V, with expected load in the range of 2 Watts. As I have just one voltage an load but the part has two channels I was hoping that I might be able to parallel them to reduce the voltage burden.
While the datasheet mentions “multiple high-side switches,” I find no information as to how this should be implemented.