I have a customer using the TLV70450 LDO. Vin = 12V, Vout = 5V @ 50mA. 12V feeds two 1uF, 25V ceramic caps through a 100 ohm resistor. Across the inputs is a 22V TVS. The output has a 4.7uF 25V ceramic.
They would like to you hear your take on the following DFMEA questions:
1. What happens when the TLV70450 GND (Pin 1) fails open?
2. What happens when the INput and OUTput pins are shorted (Pin 2 & Pin 3)?
Please let me know.
Thanks, John Garrett, TI-AFA