Hi! I'm designing a power supply for a system. As a DC-DC converter I am using the TPS63000 for a 5.5V output. I have had some problems with the feedback capacitor (Cff) that is recommend to put in parallel with R1. The recommended value for this capacitor is Cff = (2uS) / R1, whereby I get Cff = 1pF approximately. However there seems to be parasitic capacitances that affect the operation of the circuit (sometimes it works and sometimes not). Also when it does not work the integrated seems to emit a very sharp sound and overheating. Will I need to do a tuning of this capacitor? Can someone give me some information about this?
Attached is a portion of the TPS63000 data sheet:
Thank you for your help!