Other Parts Discussed in Thread: BQ24296
Hi,
i need to design a system where normally i have dc power connected to it and only when its removed, i need to use back up battery.
Other limitation comes from temperatures. Battery can be used only until +60 degrees, but the system can be running with dc power until +85 degrees.
Now, when using BQ25060 and setting charging temperature windows from 0 to +45 degrees. If temperature goes outside this window, charging is stopped. Does it mean that IN is disconnected from OUT?
If so, I cannot use this kind of approach? Is there some other way to keep dc power on continuosly when available (-30 to +85degrees) and use back up battery when needed (-10 to 60degrees, charging 0 to 45degrees)
Do I have same problem when using i.e. BQ24296 or do I have more options?
Marko