Tool/software: WEBENCH® Design Tools
Dear TI Support,
I'm really an FPGA/CPLD VHDL and Verilog designer. I took over a board that was mostly completed. I inherited the LM25118 part of the design which was already laid out and routed.
I just got in my first boards which used a Webbench generated reference design for the LM25118.
The design is for 12V output at 3A. The input is 12-36V.
The power supply feeding the design was set for 25V at 2A. The output is about 0.2V, and eventally the HB FET smoked. I checked the schematic and the value of Cboot was not correct. It is supposed to be 100 nF, but it is 180pF. Would this cause the FET to fail? Why?
Also: The reference design specifies a 100nF capacitor for Cinx X7R Kemet C0805C104K5RACTU ESR = 64,0 mOhm, VDC = 50.0 IRMS=1.64A. The capacitor specified for Cboot is a Yageo X7R CC0805KRX7R8BB104, 100nF VDC=25V IRMS =0.0A, can I use Cinx capacitor for Cboot? I have some extra parts. What is IRMS?
While I have your attention: Is there a grabber test lead that is small enough to hook onto one of the pins? Could you recommend anything?
Thank you very much for all of your help and support.
Jeff Cohen Hytorc Inc. Mawah, New Jersey USA