Other Parts Discussed in Thread: TPS63000, TPS63050, TPS62730, TPS61291, TPS62740
I've looked at TPS62743 for some time.
I am wondering if there is anything similar that also has a boost output in series with the buck?
That is to say, the power goes from a 3V battery to either the boost or buck, and then output of that goes to the other... so either battery -> buck -> boost, or battery -> boost -> buck. I suppose a boost with an integrated LDO could work too.
Target voltage is 2.1V, but we would be open to other voltages between 2.5V and 2.1V.
Thank you for help!