This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65912: Equivalent device with a different package to use in ToF reference design

Part Number: TPS65912
Other Parts Discussed in Thread: OPT9221, OPT8241

I am having a tough time finding manufacturer to fabricate board for 0.4mm pitch BGA. I would like to know if there is a equivalent device that can replace TPS65912, but with 0.5mm pitch or bigger?

I am using it in the Time of Flight reference design, with OPT9221 and OPT8241

  • Hi A.A,

    I am happy to help, I will need sometime to look into this. However, I want to confirm from your statement above that you are using the schematic that was provided in the ToF TI reference design? Otherwise, would you mind providing your schematic over a private message or email. I want to ensure I don't miss any rails. Also, I can't guarantee that there will be a one chip solution that meets your needs and is pin-to-pin compatible. If this is the case have you considered other alternatives, multi-chip solution?

    -Raymundo Hernandez-Toscano
  • Yes, I am using the ToF TI reference design schematics. And multi-chip solution is also considered.

    Much appreciated!