This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24296M: Vref for I2C configuration

Part Number: BQ24296M


I'm using BQ24296M to charge a single cell li-ion battery.  Question I had from the datasheet it was not too clear was that the I2C lines (SDA, SCL, INT) had 10k resistor pull-up to a Vref.  The datasheet does not define what that Vref is.  I saw there was some mentioning regarding 1.8V on the signals' min and max input/output voltages.  

Does the Vref have to be 1.8V or can it be greater, i.e. same voltage that powers the BQ24296M?

 - Jackson