This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27411-G1: Bq27411 Calibration problem.

Part Number: BQ27411-G1
Other Parts Discussed in Thread: BQSTUDIO

Hi, TI,

If the current accuracy is -600mA, it will be 11mA. (± 3mA for IC SPEC)
Current CAL ... bqstudio does not have a window to do cc offset cal.
In bqstudio, we calibrate manually using 'board offset' & 'pack calibration'
It is possible to do
DATASHEET also has no CMD for CAL ...
If you have CC calibration method, please reply.

Thank you.

  • Hi,

    To do the CC Cal, you will have to go to the "Data Memory" window, and on the side you will see different contents such as 'Configuration', 'Gas Gauging', 'Ra Tables', 'Calibration', and 'Security'.

    Go to 'Calibration', and you will find the CC Cal tab.

    Hope this helps,