Hello,
Here’re few design questions would like to check.
Customer need a simple control by CPU to notice this DRV for LED action.
So the INT is set NC, but I would like to check CLK_32K and TRIG.
Spec: A trigger I/O and 32-kHz clock input allow synchronization between multiple devices.
What’s the detail behavior of TRIG pin? And is the CLK 32Hz really necessary when I use just 1 driver?
My setting now is TRIG =GND, CLK=32KHz input. Thank you.
BR
Patrick