Part Number: LM5037
Hi,
I am using LM5037 circuit for my circuit. I wanted to test it in open loop to see it operates properly. The TINA simulation works perfectly for my circuit in open loop. But the hardware doesn't seem to behave as expected for the same configuration. Currently I have moved away from my PCB and am testing the circuit on breadboard. The issue still persists. I am using the application circuit provided in the datasheet(300kHz oscillator frequency). I have shorted the RES and CS pins to ground. Any suggestions to run the circuit in open module would be helpful.
I have tried providing a smal voltage value at the COMP pin and also connecting a resistor. In every case the PWM output does not come out even if all the intended signals are what they are supposed to be according to the simulation model from TINA.
I look forward to suggestions.
Thanks,
Puneeth