Hello Team,
The following specification is in the data sheet.
-------------------------------------------------------------------------
1 Features
"High 2.5-A Source and 5-A Sink Peak Drive Currents at 18-V VDD"
7.5 Electrical Characteristics
ROH(OUTH, pullup resistance) : 20Ω(max)
ROL(OUTL, pulldown resistance) : 1.25Ω(max)
-------------------------------------------------------------------------
When High flows 2.5A, I think that the power consumption will be as follows.
Will not the internal circuit be destroyed?
P=20 * 2.5 * 2.5 = 125W
Best regards,
Kato