PB_IN and nRESET are connected to "Always-on supply" in datasheet P17 9.2 Functional Block Diagram.
Where this "Always-on supply" is connected to in this IC ?
Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The "Always-On Supply" is essentially VSYS, but it is the internal voltage that supplies VSYS (also referred to as VIN).
This voltage can be supplied by AC, USB, or BAT (BAT is the primary supply to the system), so it can range from the UVLO voltage to OVP at around 6.5V
This is on Page 12 in the Logic Levels Electrical Characteristics section of the datasheet.