Other Parts Discussed in Thread: TPS92515, TPS92513,
Hello i am a german engineer an i will use the device above with many LED from the same type on the same String (connected all LEDs in one line)
For this i will use 60VDC as voltage supply.
Question 1:
In the case if i use infrared LED (730nm with nominal currend of 350mA-700mA) any LED have minimum about 1.6V.
Maximum my be 2.2V at 700mA. In other word, maximum of 26 or 27 LEDs of this type.
Is this possible?
Question 2:
for low EMI/EMV and Dimming (with PWM) , is the current flow in the LED line after inductor also ON/OFF Switched (PWM) and if yes what can i do to change this.
Because, if the current is also switched, with long line PCB distance a make an unwanted radio station :-(
Best regard from Germany
P.S. Sorry, my english is far away from perfect level