Hi team,
In the datasheet there is an equation for calculating resultant switching frequency for given Rosc, and then there is a ncie graph. The problem is they do not match.
Plug in 160 for Rosc and you get 1128kHz, more than 10% off from the graph. Why is this the case, and can you recommend the more reliable approach of the two?
If my customer wants a very specific switching frequency, are they just going to have to guess and check until they nail it?
Thanks,
Brian