This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A8300: OK to use external margin (like UCD90320) with ANYOUT FB divider?

Part Number: TPS7A8300
Other Parts Discussed in Thread: UCD90320

Hello,

I want to use the margining functionality of UCD90320, effectively a DAC back into the LDO's FB node, to margin the TPS7A8300 output @ 1.2V +/- 5%.

Is there any issue driving into FB this way? Will the LDO try to 'correct' versus what it expects from the ANYOUT configuration, or can I effectively treat the internal resistors as a passive resistor divider?

Thanks,

Jonathan