Part Number: BQ24100
Other Parts Discussed in Thread: BQ24100
OK this is my send time around . I am performing FA on our home charger for one of our electronic monitoring devices. we have been getting them back form the field with burnt up boards and the chips are pretty much destroyed. I have discovered that the input pins as well as the output pins are shorted to Pgnd pin 17 and 18 which is tied to are board ground. any way our TE groups has created a tester for the charger. The input current I m measuring is1.4 A is that acceptable for this part I can find nothing in the spec in regards to input current limits. that is question number one what is the maximum input current allowed. Could the FETs get damaged with that input current at 1.4A. I know the output is rated for 2.2A. Have any other customer seen anything similar with this part? I am trying to find a root cause for the failure.