This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM5175: lm5175 is not supporting more than 4A of current ,

Part Number: LM5175


Tool/software: WEBENCH® Design Tools

we designed the board for 12v 8A buck boost on LM5175,

but the board is not supporting more than 4A of current (ONLY 47 WATTS OF POWER) ,

The output voltage Vout  is reduced to 9v from 12v when we increase the load more than 4A ..

please suggest us the solution for this problem thanks in advance