Part Number: BQ20Z655
Hello,
i have a problèm too starte communication with the BQ20z655. the BQ evaluation softwear did not detect it . see m'y schema in attache case.
can someone helpe me.
Jedda Hamdibq20z655 (1).pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ20Z655
Hello,
i have a problèm too starte communication with the BQ20z655. the BQ evaluation softwear did not detect it . see m'y schema in attache case.
can someone helpe me.
Jedda Hamdibq20z655 (1).pdf
Hi Jedda,
What are you using the attempt communication? Are you using an EV2300 or EV2400? What is the message you get when you launch bqStudio?
Also, just to make sure the device is powering up correctly, can you please measure the voltages on the REG33, REG25, /MRST, SMBD, and SMBC pins?
Hi dMAX,
I use EV2300, the message is that he did not dectect the device.
i did not have reg33 and reg25. I saw in the datasheet that it was necessary to put a capacitor on reg33 and reg25. I miss the one of reg33 I will put it tomorrow to try.
thanks