Hi,
I currently designing a batteries pack for 4s cells Li-SOCl2 from SAFT (LSH20).
This pack should give to the user a SOC information with 5% error.
The user could change cells but some times with unknow SOC.
The user will have no boutton, only SOC display.
It seem that the BQ35100 could determine the SOC for LI-SOCI2 cells.
The datasheet sugger to use EOS mode for this kind of cells.
But in EOS mode the user have to send NEW_BATTERY() command for optimal accuracy (DATASHEET) when fresh cells will be inserts.
How to know if the cells are full or new before insert checking with gauge ? Vicious circle ?
Should I send the command when the pack open and close and the voltage measure by the BQ35100 is about 4.2V ?
Is there an method for unknow SOC cell place inside the pack ?
Thanks,