Other Parts Discussed in Thread: UCC28710, LM5023
May you pls assist me to find a reference design for following smps?
Vin 85 - 265v ac 50hz
vout- 14 V 5A isolated
Regards
Joshi
Shree Goriya Systems
New Delhi
India
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
This reference design is close to what you are looking for, Joshi.
www.ti.com/.../PMP10350
85-265VACin to 12V 5A isolated output. 60W
You are asking for 14V 5A, 70W, so this is close.
UCC28710 is the controller.
There is a UCC24630EVM, and LM5023 controller, which is wide range AC in, 19.5Vout 3.33Amps, 65Watts.
www.ti.com/.../ucc24630evm-636
www.ti.com/.../sluub81b.pdf
Does this help?