Hi,
as part of a personal project, I'm looking to design an ultra-low-noise current source capable of delivering about 8-10A - it must be programmable in some form (DC voltage?) to set the current limit. Working voltage is in the range 0-20VDC. Required precision is not great - to the nearest 100mA would probably be fine.
Any thoughts on this would be appreciated - there are standard approaches using opamps + bypass FET/NPN but I was wondering what people's thoughts are.
Many thanks
Nick