This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: Is it possible to use the bq78350-R1 with stacked bq78930's for 16s support without a separate uC?

Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQ76200, BQ76930, , BQ34Z100, BQ76PL455A, BQ77905, TIDA-01093, BQ76925, TIDA-00449

I am designing a BMS that needs to support 8s to 16s configurations. I want to use the bq78350-R1 with 2 stacked bq76930's and the bq76200 high-side FET driver. Is there any way to use qty. 2 bq76930 AFE's stacked with a bq78350-R1? I do not want to have an additional uC.

If this is not possible is there a recommended AFE that can be used with LiFePO4 cells and the bq34z100? My looking around did not find anything but I could have missed something.