Hello All,
I am currently trying to diagnose issues that I am having with a BQ51013B during power transfer. I am not getting a regular 5V output on the OUT line, instead it is floating around 1.5V while on the TX coil. When I watch the RX and TX coils during startup, the control loops appears to fail to lock in on a resonant frequency for power transfer. I measured the "Ls" and "L's" coil inductance as detailed in the BQ51013B datasheet (11.814 uH, 11.027 uH respectively). When I ran the numbers I found that we should have C1 and C2 values of 214.4 nF and 2.322 nF. In our system, C1 is currently 183 nF and C2 is 1.9nF. Is that difference between the ideal and implemented C1 and C2 values enough to throw off my wireless charging system?
Best regards,
Eric