Part Number: TPS53313
Dear sir:
I found problem with following circuit when the initial current load is ~1A. current load is permanently connected at output.
When VOUT_EN is on, the vout is 4V which generate 1A on 4ohm load. The hiccup occurs as below image and voltage never goes up.
But if I connect the load after power up, the voltage output is normal.
Thank you!