Other Parts Discussed in Thread: BQ29700EVM, CSD16301Q2, CSD16406Q3
BQ29700EVM user guide shows that discharge current typical is 1A, and maximum at 5A. When I try the circuit with discharge current at 2A, the circuit triggers the over current protection threshold. My application needs load current at 2.0 – 2.2A. Is there a way setting the over current threshold externally? Or I have to replace the on board FET?
Thanks,
Hong Liu