I have incorporated BQ25895 into a design where a high current load is driven from the battery - to drive the load V+ from the battery is connected to that load, while the main system load is powered through VSYS into an LDO with only ground common between the two power systems - is there any chance the high current return directly connected to the battery will effect the chargers internal current limits? I realize thermal control on the PCB is an issue/concern/consideration, and we've accounted for dissipation of heat, but I'm wondering if there is anything else I should be cautious of and if this "load sharing" for lack of a better term, is going to cause any issues (like if you use two transformers and don't couple both of them to the same ground...)