Hi,
I have a BQ34z100 set in HDQ mode, communicating with a MSP430. All seems OK most of the time. Occasionally, once every few hours, we get a bad read of the current (can be in DSG or in CHG) from the BQ34z100.
The number read is "24587" which in turn leads to an over current charge trip. Strangely the problem only occurs when the device is sealed. Un sealed no problems.
As recommended we have applied a fair degree of sanity checking to the HDQ comms, but there are limits to this.
Is there any relevance to the "24587" read back? IS TI aware of a solution to the problem?
Thankyou.
Regards
Martin