Other Parts Discussed in Thread: TPS25942A, TPS25944A,
Hi,
I am loading my output of the chip using a DC Electronic load with 4A at 20V. My enable input to the chip is controlled by a microprocessor. Upon power up I am able to drive the full load through the chip but if I toggle the enable (i.e. apply 3.3V and then pull it back down) then I cannot drive anything greater than 0.5A at 20V.
I am aware of the current limiter issues as discussed here and here but neither of these issues seemed to have addressed my problem. Is there something I am missing?
Thanks,
Ari