Hi,
First time here so I'm not sure if this is the right place.
I have a design that uses a regulator with input from 4.5 to 12.5V, output 3.3V. I need to update the design to use 5V from USB as an input, 3.3V output. I'm looking at the UA78M33CDCYR. Is this the right family?
I don't see an explanation in the datasheet for the letters trailing 33. What do these mean?
Thanks,
Dave