This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5170-Q1: LM5170-Q1 Design Calculator (ZIP630KB ),07 Dec 2016 Results do not match Datasheet.

Part Number: LM5170-Q1
Other Parts Discussed in Thread: LM5170

Equation 14 and 63 in the LM5170-Q1 Datasheet says: 

RRAMP = 9.6 / (FSW  * CRAMP) = 9.6 / (100000 Hz * 0.000000001F) = 96000 Hz

However in the LM5170 Design Calculator if I put in 100 kHz in Selected Switching Frequency (Cell B21) and 1 nF in Selected RAMP Capacitor (CRAMP1, CRAMP2) (Cell B62)


Calculated RAMP Resistor (RRAMP1, RRAMP2) (Cell B63) is 100.00 kOhms.

Why is it not 96 kOhms?