Other Parts Discussed in Thread: LM5166
Tool/software: WEBENCH® Design Tools
Hi,
there must be an error in the webench for this part.
Trying to replicate a design condition which is found in the datasheet WEBENCH says the design would be unstable:
For a new design instead, I get a violation of minimum on time when I reduce the minimum input voltage from 12 to 10:
but this must be wrong for sure because minimum on time depends on the max input voltage and this is already wrong at 40V:
D = 5.5/40 = 13.75% => ton = 70ns < ton_min = 95ns !!!
BR,
GPEDomotica