Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC6C598-Q1: TLC6C598-Q1 Available PWM dimming ratio

Part Number: TLC6C598-Q1

Hi,

Let me confirm about below.

--

"When data is high, the DMOS transistor outputs are capable of sinking current. This pin also can be used for global PWM dimming."

According to datasheet there is above description in "8.3.7 Output Control".

This means user can perform PWM dimming for LED.

However, there is no description about PWM dimming ratio.

I think that this spec is related to AC spec of "RCK" pin. (Ex, if user require PWM=100Hz w/ 10 bit(1024 shades of gray), then frequency for "RCK" should be 102.4kHz. (I'm not sure 102.4KHz is available for "RCK"...))

But, specification for "RCK" is NOT described in datasheet as well.

So, could you please tell me there is limitation for gray level ?

Best Regards,

Machida