This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24050: Charge current is not change

Part Number: BQ24050

Hello Support Team,

Design for BQ24050 is as the attached - for Adaptor input detection

/cfs-file/__key/communityserver-discussions-components-files/196/7266.BQ24050.pdf

- But output current for charging is always 100mA when power up (if I hot plug VBAT to 12V DC external source)

- Output current for charging is ~ 250mA (same as ISET register value) if I use a switch to On/off VBAT to 12V DC external source.

Please help me on this issue. Thanks.

Regards,

Tran Dinh Nguyen