This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2115A: Current consumption

Part Number: TPS2115A


Hello all, 

Question: 

When D0 is high

 

2.       And D1 is low

 

3.       And IN2 is active (4.2V)

 

4.       But IN1 is inactive (0V)

 

5.       AND there is no current drawn from OUT

 

6.       What is the current consumption from IN2?

  • Hi Daniel,

    For this information, you can take a look at figure 11. This graph shows the amount of current consumption from an input when the other input is unpowered and there is no current load. For a supply voltage of 4.2V, the estimated current consumption is about 50uA.

    Thanks,

    Alek Kaknevicius