This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25895: VSYS and VBUS during system reset

Part Number: BQ25895

Hello,

We're developing a battery-based product where power for the whole system comes from VSYS. We'd like to be able to perform a system-wide reset by using the BATFET reset feature (enabling BATFET_RST_EN), and connect QON to the output of our watchdog. However, when a charger is connected on VBUS, VSYS isnt disconnected after a reset, since it only turns off BATFET and not the RBFET. Is there a way (ideally, using the BQ25895's pins and not I2C commands) to turn off the RBFET and therefore create a true disconnection of VSYS, both from the battery and VBUS?

Thanks!