Part Number: BQ76PL455EVM
Tool/software: Code Composer Studio
Hi,
I am using TMS570 launchpad and BQ76PL455EVM for BMS.
I will explain you the problem in the below code snippet section.
///////////////////////////////////
nSent = WriteReg(0, 107, 0x8000, 2, FRMWRT_ALL_NR); // clear all fault summary flags
int WriteReg(BYTE bID, uint16 wAddr, uint64 dwData, BYTE bLen, BYTE bWriteType)
{
int bRes = 0;
BYTE bBuf[4] = {0, 0, 0, 0};
switch(bLen)
{
case 1:
bBuf[0] = dwData & 0x00000000000000FF;
bRes = WriteFrame(bID, wAddr, bBuf, 1, bWriteType);
break;
case 2:
bBuf[0] = (dwData & 0x000000000000FF00) >> 8;
bBuf[1] = dwData & 0x00000000000000FF;
bRes = WriteFrame(bID, wAddr, bBuf, 2, bWriteType);
break;
case 3:
bBuf[0] = (dwData & 0x0000000000FF0000) >> 16;
bBuf[1] = (dwData & 0x000000000000FF00) >> 8;
bBuf[2] = dwData & 0x00000000000000FF;
bRes = WriteFrame(bID, wAddr, bBuf, 3, bWriteType);
break;
case 4:
bBuf[0] = (dwData & 0x00000000FF000000) >> 24;
bBuf[1] = (dwData & 0x0000000000FF0000) >> 16;
bBuf[2] = (dwData & 0x000000000000FF00) >> 8;
bBuf[3] = dwData & 0x00000000000000FF;
bRes = WriteFrame(bID, wAddr, bBuf, 4, bWriteType);
break;
case 5:
bBuf[0] = (dwData & 0x000000FF00000000) >> 32;
bBuf[1] = (dwData & 0x00000000FF000000) >> 24;
bBuf[2] = (dwData & 0x0000000000FF0000) >> 16;
bBuf[3] = (dwData & 0x000000000000FF00) >> 8;
bBuf[4] = dwData & 0x00000000000000FF;
bRes = WriteFrame(bID, wAddr, bBuf, 5, bWriteType);
break;
case 6:
bBuf[0] = (dwData & 0x0000FF0000000000) >> 40;
bBuf[1] = (dwData & 0x000000FF00000000) >> 32;
bBuf[2] = (dwData & 0x00000000FF000000) >> 24;
bBuf[3] = (dwData & 0x0000000000FF0000) >> 16;
bBuf[4] = (dwData & 0x000000000000FF00) >> 8;
bBuf[5] = dwData & 0x00000000000000FF;
bRes = WriteFrame(bID, wAddr, bBuf, 6, bWriteType);
break;
case 7:
bBuf[0] = (dwData & 0x00FF000000000000) >> 48;
bBuf[1] = (dwData & 0x0000FF0000000000) >> 40;
bBuf[2] = (dwData & 0x000000FF00000000) >> 32;
bBuf[3] = (dwData & 0x00000000FF000000) >> 24;
bBuf[4] = (dwData & 0x0000000000FF0000) >> 16;
bBuf[5] = (dwData & 0x000000000000FF00) >> 8;
bBuf[6] = dwData & 0x00000000000000FF;;
bRes = WriteFrame(bID, wAddr, bBuf, 7, bWriteType);
break;
case 8:
bBuf[0] = (dwData & 0xFF00000000000000) >> 56;
bBuf[1] = (dwData & 0x00FF000000000000) >> 48;
bBuf[2] = (dwData & 0x0000FF0000000000) >> 40;
bBuf[3] = (dwData & 0x000000FF00000000) >> 32;
bBuf[4] = (dwData & 0x00000000FF000000) >> 24;
bBuf[5] = (dwData & 0x0000000000FF0000) >> 16;
bBuf[6] = (dwData & 0x000000000000FF00) >> 8;
bBuf[7] = dwData & 0x00000000000000FF;
bRes = WriteFrame(bID, wAddr, bBuf, 8, bWriteType);
break;
default:
break;
}
return bRes;
}
int WriteFrame(BYTE bID, uint16 wAddr, BYTE * pData, BYTE bLen, BYTE bWriteType)
{
int bPktLen = 0;
BYTE pFrame[32];
BYTE * pBuf = pFrame;
uint16 wCRC;
if (bLen == 7 || bLen > 8)
return 0;
memset(pFrame, 0x7F, sizeof(pFrame));
if (wAddr > 255) {
*pBuf++ = 0x88 | bWriteType | bLen; // use 16-bit address
if (bWriteType == FRMWRT_SGL_R || bWriteType == FRMWRT_SGL_NR || bWriteType == FRMWRT_GRP_R || bWriteType == FRMWRT_GRP_NR)//(bWriteType != FRMWRT_ALL_NR)// || (bWriteType != FRMWRT_ALL_R))
{
*pBuf++ = (bID & 0x00FF);
}
*pBuf++ = (wAddr & 0xFF00) >> 8;
*pBuf++ = wAddr & 0x00FF;
}
else {
*pBuf++ = 0x80 | bWriteType | bLen; // use 8-bit address
if (bWriteType == FRMWRT_SGL_R || bWriteType == FRMWRT_SGL_NR || bWriteType == FRMWRT_GRP_R || bWriteType == FRMWRT_GRP_NR)
{
*pBuf++ = (bID & 0x00FF);
}
*pBuf++ = wAddr & 0x00FF;
}
while(bLen--)
*pBuf++ = *pData++;
bPktLen = pBuf - pFrame;
wCRC = CRC16(pFrame, bPktLen);
*pBuf++ = wCRC & 0x00FF;
*pBuf++ = (wCRC & 0xFF00) >> 8;
bPktLen += 2;
sciSend(scilinREG, bPktLen, pFrame);
return bPktLen;
}
////////////////////////////////////////
nSent gives the return value of WriteReg -- bRes.
bRes gives the return value of Writeframe -- bPktLen.
So, actually nSent gives the values of bPktLen.
If i am keeping bLen as 2, I am getting nSent as 6 and i am keeping bLen as 3, I am getting nSent as 7.
So, what is the relation between bLen and bPktLen ? Are they both not same?
Please help me out with understanding.
Thanks
Ritul Shah