Hi all,
My requirements:
charge (at 0.5C) Li-ion battery pack using a solar panel,
and discharge (at 0.3C) the battery pack with a load. A suitable cost effective solution!
Battery pack: 4s30p configuration of 18650 cells of 1000mAh capacity each.
Short listed IC for solar charge controller with MPPT:
BQ24650 but it has maximum charge current = 10A, I need at least 15A charge current! (charging at 0.5C)
1. Is the selection of charge controller for above battery pack configuration suitable?
2. Any other alternative for 15A charge current solar charge controller with MPPT?
3. Dose this IC support simultaneous charge and discharge of Li-ion battery pack?
For battery monitoring (4s30p 18650 cell pack):
Shortlisted three ICs:
BQ76920 BQ76925 BQ76PL536A BQ76PL536A-Q1
4. Which among them is the most suitable for the above configuration of battery pack and charge controller?
5. How to monitor 30 parallel 18650 cells?
6. Is stacking of batter monitor IC to cover all the parallel branch suitable?
7. Do I need to consider any other parameters for selection of battery monitoring IC?
8. Can these battery monitoring ICs suitable to monitor 4s30p battery pack?
9. How is behavior of the battery monitor IC when it is monitoring a 4s30p configuration of 18650 cells?
10. What could be the best suitable microcontroller for the above battery monitoring ICs?
My application is not automotive
Kindly guide me in this regard.
Thanks and regards.